s32 sonycam focal length

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32 sonycam focal length

1,340 Views
alan13341313
Contributor I

What is the focal length of it ?

I can't find answer in datasheet

0 Kudos
Reply
2 Replies

1,233 Views
andrei_skok
NXP Employee
NXP Employee

The focal length of the S32V-SONYCAM is 6,1 mm

0 Kudos
Reply

1,233 Views
fangyue
Contributor II

Hi Andrei.,

Is the focal length the same for both x-axis and y-axis? Could you also tell me the principal point and image size of S32V-SONYCAM? I need these calibration parameters for further development. Thanks in advacne.

BR,

Yue

0 Kudos
Reply