Will S32V automatically send its ID by CAN or ethernet?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will S32V automatically send its ID by CAN or ethernet?

811件の閲覧回数
Da2
Contributor I

Hello friends,

Will S32V automatically send its ID by CAN or ethernet?

BRs 

Yuan Da

ラベル(1)
0 件の賞賛
返信
1 返信

773件の閲覧回数
yangruihero
NXP Employee
NXP Employee

Dear Da:

For CAN function, S32V can support “Controller Area Network (FlexCAN)”(please refer to Chapter 40 in S32V234 Reference Manual);

for Ethernet, S32V can support “10/100/1000-Mbps Ethernet MAC (ENET)”(please refer to Chapter 43 in S32V234 Reference Manual);

For S32V UNIQUE_ID, they are located in S32V_Fuse.

S32V FlexCAN and ENET IP will not use UNIQUE_ID directly, because they are just hardware interface, UNIQUE_ID can be used by software.

By the way, we have not heard any CAN software protocol stack or Ethernet software protocol stack will use IC’s ID.

You can check information about CAN-ID or Ethernet MAC address(IP address) from website.

Thanks.

0 件の賞賛
返信