Where can I find xdm containing os event, task?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find xdm containing os event, task?

3,130 Views
decoski
Contributor II

When I was reading the manual 2.4_Studio_documentation_developers_guide and planning to build a configuration project according to Os_TS_T40D2M10I0R0, I chose the Os module. I found that the Os module only has OsCounter.

122.png

How can I get the task, event and other configurations in the manual, and where can I download the Os (4.1.0 AS4.0.2) in the manual?

123.png

Thanks for the support!

Labels (1)
Tags (1)
0 Kudos
Reply
7 Replies

3,118 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi decoski,

In the MCAL package and RTD package, the Os module is a stub.
To use Os, you can download the OS packages at this link:
https://are.nxp.com/FlexNetCatalog.aspx
Or you can contact EB Elektrobit to get support for this issue.

Best regards,

Dan

0 Kudos
Reply

3,106 Views
decoski
Contributor II

Thank you for your reply, but I seem to be unable to open this link. Can you send a copy to me, thank you!

0 Kudos
Reply

3,097 Views
DanNguyenDuy
NXP Employee
NXP Employee

Dear decoski,

I think you can open this link if you had an account on the nxp.com website. Could you capture your screen when you open the link?

Best regards,

Dan

0 Kudos
Reply

3,077 Views
decoski
Contributor II
Shows as follows:
Hmm... Can't access this page to check are.nxp.com for spelling errors.
If the spelling is correct, try running Windows Network Diagnostics.
DNS_PROBE_FINISHED_NXDOMAIN
0 Kudos
Reply

3,051 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi decoski,

If you can not access the website.

I think you should try another way: contact EB Elecktrobit to ask about your OS error.

Best regards,

Dan

0 Kudos
Reply

3,038 Views
decoski
Contributor II
My other colleagues including overseas friends can't open this link. Why can't you provide a valid link or send me a copy? I don't have an account on eb that can be supported. Can you provide me with an effective help, thank you
0 Kudos
Reply

3,012 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi decoski,

I discussed your issue with my colleagues. Sorry because I provided you the website is accessible by NXP employees only.

The last version of the Autosar OS 4.0 is available through search https://www.nxp.com/search?keyword=+AUTOSAR+4.0+OS+%28QM%29+for+S32K14x&start=0

The direct download link is then  AUTOSAR 4.0 OS (QM) for S32K14x

Best regards,

Dan

0 Kudos
Reply