VisonSDK 1.3 demo apps apex_isp_ldw_cv can't build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VisonSDK 1.3 demo apps apex_isp_ldw_cv can't build

3,287件の閲覧回数
alan13341313
Contributor I

In file included from ../../../../../isp/graphs/imx224_exp_ctrl/src/imx224_exp_ctrl.c:34:0:
./kmem.c:3:21: warning: backslash-newline at end of file
char kmem_srec[] = {\

./kmem.c:4:1: warning: missing terminating " character
"\
^
./kmem.c:4:1: error: missing terminating " character
../../../../../isp/graphs/imx224_exp_ctrl/src/imx224_exp_ctrl.c:39:1: error: expected expression before ‘static’
static SEQ_FdmaCfg_t FastDMA;
^~~~~~
../../../../../build/nbuild/helpers.mk:156: recipe for target 'imx224_exp_ctrl-c.o' failed
make[3]: *** [imx224_exp_ctrl-c.o] Error 1
make[3]: Leaving directory '/home/kevin/NXP/S32DS_Vision_v2018.R1/S32DS/s32v234_sdk/isp/graphs/imx224_exp_ctrl/dynamic_imx224_exp_ctrl/build-v234ce-gnu-linux-o'
../../../../../build/nbuild/sub.mk:73: recipe for target 'allsub' failed
make[2]: *** [allsub] Terminated
make[2]: Leaving directory '/home/kevin/NXP/S32DS_Vision_v2018.R1/S32DS/s32v234_sdk/isp/graphs/imx224_exp_ctrl/dynamic_imx224_exp_ctrl/build-v234ce-gnu-linux-o'
../../../../build/nbuild/sub.mk:73: recipe for target 'allsub' failed
make[1]: *** [allsub] Terminated
make[1]: Leaving directory '/home/kevin/NXP/S32DS_Vision_v2018.R1/S32DS/s32v234_sdk/demos/apps/apex_isp_ldw_cv/build-v234ce-gnu-linux-o'
/home/kevin/NXP/S32DS_Vision_v2018.R1/S32DS/s32v234_sdk/build/nbuild/platforms/coordinator.mk:57: recipe for target 'allsub' failed
make: *** [allsub] Error 2

タグ(4)
0 件の賞賛
返信
2 返答(返信)

3,105件の閲覧回数
liujinbao
Contributor II

hello,

You find the file kmem.c to see if there is a problem with this file.

0 件の賞賛
返信

3,105件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Yung,

The error is due to bad imx224_exp_ctr.c you must download again the  VisionSDK, btw we do have example graph for exposure control for imx224 sensor at s32v234_sdk\isp\graphs\imx224_exp_ctrl. But we don't have full fledged example in VSDK.So you can take reference from isp_ov10640_default demo and port it to work with imx224 using imx224_exp_ctrl graph.

Regards

0 件の賞賛
返信