Using SD-ADC in S32R274 EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using SD-ADC in S32R274 EVB

2,781 Views
samco1919
Contributor I

Hello,

I am new to NXP products and doing my first steps using the S32R274 EVB.

I am trying to implement a fast adc sampler for signal processing application. From the datasheet, the SAR-ADC maximum sampling frequency is 1MSps and the SD-ADC is 10MSps. For my application I would prefer the higher sampling frequency.

While mentioned few times in the datasheet and reference manual, I could not find any example or technical information on how to use the SD-ADC. The SAR-ADC is very straight forward with it's ready to use standalone component/ as part of the ADC-PAL. I also could not find an implementation in the RSDK.

If someone can please guide me toward an example or tutorial it would be great.

Thank you

Labels (2)
0 Kudos
Reply
1 Reply

2,645 Views
Hong_Tang
Contributor I

Hi,

I met the same problem, so could you please tell me how you figured it out? Thank you.

0 Kudos
Reply