Unable to generate code from Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to generate code from Processor Expert

3,360 Views
sushma
Contributor III

Hello,

I'm facing this issue of unable to generate the Processor expert Code, as project isn't been activated in the Project Panel. Is there any means to activate the project or any means that will solve this issue?

Thank you

image.pngimage.png

0 Kudos
Reply
5 Replies

3,167 Views
jiri_kral
NXP Employee
NXP Employee

Thanks for sharing screenshots. Processor Expert is part of SDK and your project (example) is not based on SDK. 

You can use SDK ADC example insdead: 

pastedImage_1.png

Jiri

0 Kudos
Reply

3,167 Views
sushma
Contributor III

pastedImage_1.png

Hello,

 I don't have the following example(attached screenshot) and my purpose is to generate using processor expert. Have to integrate it with other auto generate code. Can you suggest me any solution.

Thank you

0 Kudos
Reply

3,167 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

Did you update your S32DS installation? https://community.nxp.com/docs/DOC-341068 

Even with non-updated S32DS installation you can use ADC example with Older SDK (just scroll more down in example list). The example which you are using is non-SDK example. 

Jiri 

0 Kudos
Reply

3,167 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

your screenshots are no more available. Can you please share it again? 

Jiri 

0 Kudos
Reply

3,167 Views
sushma
Contributor III

pastedImage_1.pngpastedImage_2.png

0 Kudos
Reply