Unable to generate code from Processor Expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to generate code from Processor Expert

3,299件の閲覧回数
sushma
Contributor III

Hello,

I'm facing this issue of unable to generate the Processor expert Code, as project isn't been activated in the Project Panel. Is there any means to activate the project or any means that will solve this issue?

Thank you

image.pngimage.png

0 件の賞賛
返信
5 返答(返信)

3,106件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Thanks for sharing screenshots. Processor Expert is part of SDK and your project (example) is not based on SDK. 

You can use SDK ADC example insdead: 

pastedImage_1.png

Jiri

0 件の賞賛
返信

3,106件の閲覧回数
sushma
Contributor III

pastedImage_1.png

Hello,

 I don't have the following example(attached screenshot) and my purpose is to generate using processor expert. Have to integrate it with other auto generate code. Can you suggest me any solution.

Thank you

0 件の賞賛
返信

3,106件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

Did you update your S32DS installation? https://community.nxp.com/docs/DOC-341068 

Even with non-updated S32DS installation you can use ADC example with Older SDK (just scroll more down in example list). The example which you are using is non-SDK example. 

Jiri 

0 件の賞賛
返信

3,106件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

your screenshots are no more available. Can you please share it again? 

Jiri 

0 件の賞賛
返信

3,106件の閲覧回数
sushma
Contributor III

pastedImage_1.pngpastedImage_2.png

0 件の賞賛
返信