The generated port is not sorted with Pin Name via S32 Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The generated port is not sorted with Pin Name via S32 Design Studio

494件の閲覧回数
WQS
Contributor I

Hello TechTeam,

We want to generated port which is sorted with Pin Name, but it is not. If there have any way to comply this requirement.

We sort all ports according Pin Name in S32DS:

WQS_0-1714983831109.png

But the generated code is not sorted with Pin Name, and the first one should be the PORTD1, not the PORTA0:

WQS_1-1714983976690.png

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)