The Can controller cannot receive and send with S32R418AA。

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The Can controller cannot receive and send with S32R418AA。

跳至解决方案
2,032 次查看
RanDong
Contributor I
I can't send and receive properly with the controller, and I caught the chip pin with the logic analyzer without any changes. Whether there are other Settings.20230904-113003.jpg20230904-113016.jpg20230904-113020.jpg
标签 (1)
0 项奖励
回复
1 解答
1,976 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is sequence of error frames sent due to bit error, because FlexCAN does not see a same bit as is sent. Module does to bus off and recover automatically (by default). Most probably CAN transceiver is not active, check board's schematic
this is for rev.B

PetrS_0-1693909500687.png

Be sure EN, STB are held high, or remove jumpers.
You can also try to remove TXD/RXD jumpers and connect PC8, PC7 together and send message. If pins are properly initialized then you should see message transmitted still.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,003 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

setting looks normal. If right pin is selected, be sure connected CAN transceiver is active and bus terminated, connect other node with same bitrate setting. Measure with scope/analyzer TXD/RXD and CAN bus signal. Also check within debugger module's ECR/ESR1 registers to know if any error is detected.

BR, Petr

0 项奖励
回复
1,979 次查看
RanDong
Contributor I

I caught the controller's TX signal as follows.The baud rate is 500K.Can you help me see how it happened.1.jpg

@PetrS 

0 项奖励
回复
1,977 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is sequence of error frames sent due to bit error, because FlexCAN does not see a same bit as is sent. Module does to bus off and recover automatically (by default). Most probably CAN transceiver is not active, check board's schematic
this is for rev.B

PetrS_0-1693909500687.png

Be sure EN, STB are held high, or remove jumpers.
You can also try to remove TXD/RXD jumpers and connect PC8, PC7 together and send message. If pins are properly initialized then you should see message transmitted still.

BR, Petr

0 项奖励
回复
1,935 次查看
RanDong
Contributor I
This issue has been resolved,Thanks.
0 项奖励
回复
1,986 次查看
RanDong
Contributor I
Hi,
The value of the register indicates that an error was sent into busoff.can you provide me with a routine that can be sent normally.I can't find anything wrong here.Emulation board is S32R41.

Thanks.
0 项奖励
回复