Spi with DMA problems in S32K344 using design studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Spi with DMA problems in S32K344 using design studio

1,093 次查看
Rmpr
Contributor II

Hello,

I'm having problems sending an array with lpspi using dma.

I'm trying to send this array 5 times:

 

 

uint8 TxMasterBuffer[NUMBER_OF_BYTES] = {0xA5, 0xA5, 0x6, 0xA5, 0x7};
for(int i = 0; i<5; i++){
    	Lpspi_Ip_AsyncTransmit(&SPI_EXTERNAL_DEVICE, TxMasterBuffer, RxMasterBuffer, NUMBER_OF_BYTES, Lpspi_Ip_Callback);
    }

 

 

 

The problem is that it only send one time the array. When I debug it changes the received buffer but in oscilloscope I can only see one message.

 

Is it a problem with configuration or the dma can't support this operation? I'm using the lpspi RTD's.

 

标签 (1)
0 项奖励
回复
1 回复

1,071 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Do not call Lpspi_Ip_AsyncTransmit so frequently. Otherwise, I think the next few calls of Lpspi_Ip_AsyncTransmit cannot return LPSPI_IP_STATUS_SUCCESS.

Please call Lpspi_Ip_AsyncTransmit again in LPSPI_IP_EVENT_END_TRANSFER of Lpspi_Ip_Callback.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复