[Security] The I/F used by the secure boot trust chain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Security] The I/F used by the secure boot trust chain

Jump to solution
1,544 Views
Gideon
Contributor III

Dear NXPs:

My Flash layout is as shown below:

 

My trust chain is like this:

1.CSEc boot ROM verifies the bootmanaer image, and executes bootmanaer after verification.

2.The bootmanager verifies the bootloader and executes the bootloader after completion.

3.The bootloader verifies the application and executes the application after completion.

My question is during step 2 and step 3, should I use the 0x02-ENC-CBC (AN5401) I/F of the CSEC component to calculate the CMAC values of the bootloader and application image?

Labels (1)
0 Kudos
Reply
1 Solution
1,498 Views
Gideon
Contributor III

Dear NXPs:

Taking the Application area as an example, use the CMD_GENERATE_MAC interface to calculate the CMAC value of the Application and automatically save it in CSEc. Use the CMD_VERIFY_MAC interface and the interface parameter is the CMAC value calculated on the PC (CMAC in the purple area) for verification, right?

View solution in original post

0 Kudos
Reply
3 Replies
1,509 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Gideon 

CMD_ENC_CBC command is for encryption. You need to generate and verify CMAC, so you should use commands CMD_GENERATE_MAC and CMD_VERIFY_MAC.

Regards,

Lukas

0 Kudos
Reply
1,499 Views
Gideon
Contributor III

Dear NXPs:

Taking the Application area as an example, use the CMD_GENERATE_MAC interface to calculate the CMAC value of the Application and automatically save it in CSEc. Use the CMD_VERIFY_MAC interface and the interface parameter is the CMAC value calculated on the PC (CMAC in the purple area) for verification, right?

0 Kudos
Reply
1,482 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Not sure if I can understand: "automatically save it in CSEc" - CMAC is not automatically saved to CSEc when using CMD_GENERATE_MAC.

"Use the CMD_VERIFY_MAC interface and the interface parameter is the CMAC value calculated on the PC (CMAC in the purple area) for
verification, right?"
- Yes, that's correct.

Regards,

Lukas

0 Kudos
Reply