SDK-Pin_mux Functional Properties

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK-Pin_mux Functional Properties

跳至解决方案
3,815 次查看
sohyunjang
Contributor III

Hi,

I use S32DS for ARM ver1.3.

But there are problem for Pin_mux Functional Properties.

Same problem: https://community.nxp.com/thread/453548#comment-914814

The reply is "We will come with an update on the issue as soon as we identify the root cause"

So, Has this problem been resolved?

And, I use MTRDEVKSBNK144 Application Software

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/s32-autom...

How Can I compile this application at S32DS for 2.0?

What should I modify?

Thank you.

0 项奖励
回复
1 解答
3,300 次查看
cezardobromir
NXP Employee
NXP Employee

Hello Sohyun,

This issue is not present on S32DS v1.3 and update site for S32 SDK 1.0.0 RTM release.

It has appeared on the releases that followed.

So everything should work ok if installing S32DS v1.3 and S32 SDK 1.0.0 RTM update site (update 2 from Flexera).

Please tell me if using them in this combination works fine for you.

Best regards,

Cezar

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,300 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

the MTRDEVKSBNK144  is for S32DS ARM v1.3 only. Please see MTRDEVKSBNK144 release notes. 

Jiri 

0 项奖励
回复
3,300 次查看
cezardobromir
NXP Employee
NXP Employee

Hello Sohyun,

Yes, this problem has been fixed in S32 SDK EAR 0.8.5. All the versions form this one to the present display the correct information in the Functional Properties tab

Best regards,

Cezar

0 项奖励
回复
3,300 次查看
sohyunjang
Contributor III

Hi,

I use MTRDEVKSBNK144 Application Software

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/s32-autom...


And, this Application use S32 SDK_S32K144_RTM_1.0.0.

I want to know if this problem has been fixed in S32 SDK_S32K144_RTM_1.0.0.

And, I want to know difference between EAR SDK and RTM SDK.

Thank you.

@Jiri Kral

0 项奖励
回复
3,301 次查看
cezardobromir
NXP Employee
NXP Employee

Hello Sohyun,

This issue is not present on S32DS v1.3 and update site for S32 SDK 1.0.0 RTM release.

It has appeared on the releases that followed.

So everything should work ok if installing S32DS v1.3 and S32 SDK 1.0.0 RTM update site (update 2 from Flexera).

Please tell me if using them in this combination works fine for you.

Best regards,

Cezar

0 项奖励
回复
3,300 次查看
sohyunjang
Contributor III

Hi,

I try to install S32DS Ver1.3 update 2. The issue has been resolved.

Update 4 seems to be causing problems.


Thank you.

0 项奖励
回复