S32k344 install new SDK(RTD_4.4_2.0.1) question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k344 install new SDK(RTD_4.4_2.0.1) question

1,525 Views
fxn
Contributor II

Hi 

During the installation of RTD 2.0.1, the following figure 1 appears: How to solve this problem? , When we press install anyway, the RTOS and lwip cannot be used as shown in Figure 2 below. If we normally use the SDK of the previous version of RTD 2.0.0, we can use RTOS and lwip module as shown in Figure 3 below. Could you please help to see what the problem is?

Figure 1

fxn_0-1659405463637.png

Figure 2

fxn_1-1659405504841.png

Figure 3

fxn_2-1659405525724.png

Thank you

Guanlin

0 Kudos
Reply
1 Reply

1,420 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @fxn 

Unfortunately, these latest TCP/IP and FreeRTOS packages are only compatible with RTD 2.0.0. You need to downgrade the RTD version to 2.0.0 in order to use them.

Best Regards,

Nam

0 Kudos
Reply