S32K146 UART send problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 UART send problem

3,810 Views
347996379
Contributor III

hello, SDK.

When I use the following statement, the uart cannot emit any data.But SDK routines do support this.When I add "while(UART_GetTransmitStatus(&uart1_pal_instance, &bytesRemaining) == STATUS_BUSY)" at the end of the statement, the UART can send data as normal.How to solve this problem?

UART_SendData(&uart1_pal_instance, sendbuf, size);

Labels (2)
0 Kudos
Reply
2 Replies

3,650 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 张 舜毅,

Your method is correct.

UART_GetTransmitStatus returns whether the previous transmission has finished.

UART_GetTransmitStatus.png

Have you check the status of UART_SendData? If it return STATUS_BUSY?
It is not recommend to call UART_SendData regularly, without check whether the previous transmission has finished.

UART_SendData.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,598 Views
ManuelDuran
Contributor I

Hi!

I have a problem using Uart to send a data in order to chek it with the Putty.

I am using s32k146 EVB and S32IDE, and I want to send a data by the uart to learn about this communication. I am quite new in this world. So you can see the code in the next lines:

 
 
 

/* Write your code here */
(void) CLOCK_SYS_Init (g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr,
CLOCK_MANAGER_CALLBACK_CNT);
(void) CLOCK_SYS_UpdateConfiguration (0U, CLOCK_MANAGER_POLICY_AGREEMENT);
/* For example: for(;;) { } */

pins_channel_type_t result,result2;
HAL_DIO_result_t res;
uint8_t num=3;
res=HAL_DioInit();
LPUART_DRV_Init(INST_LPUART1, &lpuart1_State, &lpuart1_InitConfig0);

for(;;){
result=HAL_DioGet(DIO_INPUT_PTC12);
if(!result){
HAL_DioSet(DIO_INPUT_PTC12, 1);
LPUART_DRV_SendData(INST_LPUART1, &num, 1);
}
else{
HAL_DioSet(DIO_INPUT_PTC12, 0);
}

}

In this code, you can see I want to send a simply uint data(m), when result =0. But I do not have any data in the Putty, when the program run the instruction of sendata. I have checked the following probably errors:

1. The putty is well configured, with the correct COM, the correct baud rate,...

2. I think the Uart12 is also well configured and initialized.

3. I think that Uart sends data using interrupts by default. I tried some ways to prove this but I didn´t have results.

4. The processor Expert is well configured. Uart1 to trasmit, output.

5. I also tried to use the function of SDK, get_TransmitStatus in order to see how the state of the process was during the trasmition, but was always success, surprisingly.

6. I compare with the lpuart example of the guide of the board, but I must use the function of SDK, such as DRV_SendData, DRV_get_TransmitStatus, etc.

7 I also tried to use the functions sendDataPolling and sedDataPolling, but I didn´t have good results.

Can you help me, please?

Thank so much.

Manuel.

 

 

 

0 Kudos
Reply