S32K144 -FlexCAN Example Not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 -FlexCAN Example Not working

3,016 Views
sakthivelkuland
Contributor III

Hi all,

I'm new to S32K144 MCU, My TPMS Application used S32K144 MCU now I have used the CAN Module for communication with other ECU.

I have considered the sample Example from Freescale Document Number: AN5413, This example not working for me when I try to see the CAN Data signals with MCU CAN_Tx pin with Scope.

My idea first take the sample example for testing with standard CAN ID Communication but this example not working for me.

Note, My project not used any SDK version. 

If anyone succeeds in FlexCAN with non-SDK Please share your code.

Thanks,

Sakthivel k

Labels (1)
0 Kudos
Reply
1 Reply

2,545 Views
nxf33121
NXP Employee
NXP Employee

Hi Sakthivel,

 

I ran that code from AN5413 and it is working properly.

The example is intended for two EVBs. Assuming you are using S32K144EVB, please follow the steps described in Example Operation section (2.9.2.5).

 pastedImage_7.png

Regards,

Carlos

0 Kudos
Reply