S32K SDK can_pal lack

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K SDK can_pal lack

跳至解决方案
2,451 次查看
adria
Contributor I

Hi,

I am usign processor expert and have added can_pal component to my project. I see there are some features from FlexCAN which can_pal doesn't cover. If I want to use them, what do you recommend me to do:

1. Keep using can_pal and, in case I want to use some of the FlexCAN functions which are not covered by can_pal, directly call those FlexCAN function.

2. Remove can_pal component from my project and start using only FlexCAN.

Best regards,

Adria

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,234 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Adria,

If your application allows you to use FlexCAN instead of can_pal, my recommendation would be to stick to your second option, remove can_pal component from your project and start using only FlexCAN.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,235 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Adria,

If your application allows you to use FlexCAN instead of can_pal, my recommendation would be to stick to your second option, remove can_pal component from your project and start using only FlexCAN.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复