S32G Linux kernel panic on pfeng module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G Linux kernel panic on pfeng module

2,741 Views
xhu
Contributor I

Hi,

I built Linux image from bsp24.0, fsl-image-base, the ddr settings were generated from S32DS tools. I saw Linux kernel panic during boot up late stage. It did not happen every time, hit this every 10-20 times power cycles. U-boot, dtb, kernel and rootfs are flashed into emmc. Please advise. The full log file is also attached.

[ 4.326893] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000060
[ 4.326895] Mem abort info:
[ 4.326898] ESR = 0x96000005
[ 4.326902] Exception class = DABT (current EL), IL = 32 bits
[ 4.326905] SET = 0, FnV = 0
[ 4.326907] EA = 0, S1PTW = 0
[ 4.326909] Data abort info:
[ 4.326912] ISV = 0, ISS = 0x00000005
[ 4.326914] CM = 0, WnR = 0
[ 4.326923] user pgtable: 4k pages, 39-bit VAs, pgdp = 00000000d3bfd33d
[ 4.326926] [0000000000000060] pgd=0000000000000000, pud=0000000000000000
[ 4.326937] Internal error: Oops: 96000005 [#1] PREEMPT SMP
[ 4.326945] Modules linked in: nxp pfeng(O)
[ 4.326958] Process rngd (pid: 873, stack limit = 0x00000000f0b17534)

Thanks,

Xiaodong

0 Kudos
Reply
1 Reply

2,609 Views
bpe
NXP Employee
NXP Employee

Based on this information, it is not possible to establish the root cause of the
problem. Kernel panic is a normal reaction to broken pointers, the fact that
it happens from time to time points towards possible  memory decay.
The suggestions therefore are, test the system memory and debug your kernel.


Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply