S32DS 2018.R1, update 10: error on new project from example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS 2018.R1, update 10: error on new project from example

2,015件の閲覧回数
gaetanocirillo
Contributor I

Hello,

as a newbie of the S32 ecosystem I would really appreciate the help of an expert :-)

I've just bought an S32K142 Eval Board and I've done a fresh install of S32DS 2018.R1, updated it as requested by the software itself, installed S32K1xx RTM SDK v3.0.0 and then I've tried to create ans S32DS project from example; but it gives me this warning:

s32ds_error.jpg

What's happening? Any help will be very welcome!

Thank you

My System information:

Win10 Pro, 10.0.17763

S32 Design Studio for ARM, Version: 2018.R1, Build id: 180815

タグ(4)
2 返答(返信)

1,859件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Gaetano Cirillo

Could you clarify how do you update the SDK software, this error could be caused by an error version of the SDK with the S32DS IDE, so you need to update the SDK software. Did you use the software:

pastedImage_1.png

For your reference:

https://community.nxp.com/message/1097574 

Hope this helps

Best regards

0 件の賞賛
返信

1,859件の閲覧回数
ww34ww34
Contributor I

Hi Gaetano, 
I have the same issue, the same identical conditions. Can't figure out how to solve it.
I hope in the help of something more expert than us
Which packages have you installed?

0 件の賞賛
返信