S32 SDK for MPC5775K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 SDK for MPC5775K

1,664 Views
priyan_george
Contributor I

Hi,

I am using S32 studio Version: 2.1 . I am not able to add FreeRTOS OS component to MPC5775K project.External SDK added for MPC5775K is AMMCLIB_1.1.15.

The S32 external SDK available are

- S32_SDK_S32PA_RTM_3.0.0

- FreeMASTER_Serial_Communication_Driver_V2_0

- AMMCLIB_1.1.15

I was able to add freertos ,os component ,for MPC5775E , which was under external SDK S32_SDK_S32PA_RTM_3.0.0.

Can I get SDK support for MPC5775K under  SDK S32_SDK_S32PA_RTM_3.0.0 , so that I can use FREERTOS with MPC5775K.

Labels (1)
0 Kudos
Reply
2 Replies

1,560 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I will add that MPC5775K is not recommended for new designs, so there won't be SDK for this part. For replacement, see please S32R devices:

S32R Radar MCUs | NXP 

Regards,

Lukas

0 Kudos
Reply

1,560 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

Unfortunately MPC5775K is not supported by SDK:
pastedImage_1.png

Jiri

0 Kudos
Reply