S32_SDK_S32K1xx_RTM_4.0.0.exe is installed, how to deploy in S32DS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32_SDK_S32K1xx_RTM_4.0.0.exe is installed, how to deploy in S32DS?

3,726 次查看
my_souls
Contributor III

I am currently using S32DS for arm V2.0. After installing S32_SDK_S32K1xx_RTM_4.0.0.exe, I cannot find the S32_SDK_S32K1xx_RTM_4.0.0 example in the creation example.

how to deploy in S32DS?

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

3,615 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kun Liu,

After download and install the S32_SDK_S32K1xx_RTM_4.0.0, I was able to see the S32SDK_for_S32K1xx_RTM_4.0.0_ReleaseNotes in folder (C:\NXP\S32_SDK_S32K1xx_RTM_4.0.0).

S32SDK_for_S32K1xx_RTM_4.0.0_ReleaseNotes.png

The "6.3 Compiler and IDE versions" shows that the S32 Design Studio 3.3 IDE support S32_SDK_S32K1xx_RTM_4.0.0. 

 

Moving forward the support for S32K1xx / S32K1xxW will be integrated as part of the S32 Design Studio for S32 Platform. You can find the latest version (v3.3 released June 2020), in the Downloads tab of this IDE variant:

S32 Design Studio | NXP 

S32 Design Studio 3.3.png

 

Unfortunately:

There are still some errors when build the project of SDK4.0.0 using S32DS 3.3. 
"By default, There was no platform integrated in S32DS. In order to use S32DS for S32K1xx. Users need to install the development package for S32K1xx but this package is from another team We are in discussion with that team to request them publish it"

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,614 次查看
my_souls
Contributor III

Hi Robin Shen:

    OK, I hope it can be released soon, thank you very much!

0 项奖励
回复

3,614 次查看
razva_tilimpea
NXP Employee
NXP Employee

Hi Kun,

All updates for RTM 4.0.0 are available in Design Studio as update sited. Please check and let us know if you have other issues.

Best regards,

Razvan

0 项奖励
回复