S32 Design studio with FreeRTOS v10.0.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design studio with FreeRTOS v10.0.1

跳至解决方案
3,368 次查看
alternativeunof
Contributor II

Hi everybody,

I want to ask you if is possible to update the the S32K SDK with the new version of FreeRTOS v10.0.1, and so to update also the processor expert for the new component in S32 Design Studio.

I need this new version of FreeRTOS since the one provided with the SDK (v8) does not provide static memory allocation, which must be used for safety critical application.

If there is no way to update both sdk and component, can you describe to me a method to manually integrate FreeRTOS v10.0.1 into the existing SDK along with the new component for the processor expert?

Thank you.

1 解答
2,707 次查看
BlackNight
NXP Employee
NXP Employee

Hi Igol,

the following tutorial might be what you are looking for:

Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1 | MCU on Eclipse 

I hope this helps,

Erich

在原帖中查看解决方案

1 回复
2,708 次查看
BlackNight
NXP Employee
NXP Employee

Hi Igol,

the following tutorial might be what you are looking for:

Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1 | MCU on Eclipse 

I hope this helps,

Erich