Run sdk makefile project example error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run sdk makefile project example error

2,908 Views
lognight
Contributor III

I ran the example of using makefile project in D:\NXP\S32DS_Power_v1.2\S32DS\S32_SDK_MPC5748G_EAR_0.8.0\examples\MPC5748G\demo_apps\hello_world-mkf\GCC-MKF, met an error as following, how can I slove this problem.

I using  S32DS_Power_v1.2.

100.PNG

0 Kudos
Reply
2 Replies

2,732 Views
stanish
NXP Employee
NXP Employee

Hi Steven,

Thanks for this report. 

I suspect there is an issue in the example makefile which does not work well with the latest GCC compiler (S32DS Power v1.2)

Could you possibly try to remove the linker options below from the Makefile (line 124, 127):

-nostartfiles
-nostdlib
<S32DS_Power_v1.2>\S32DS\S32_SDK_MPC5748G_EAR_0.8.0\examples\MPC5748G\demo_apps\hello_world-mkf\GCC-MKF\Makefile

## Linker flags
LDFLAGS_RAM:=-Wl,-Map=$(MAP_RAM)
LDFLAGS_RAM+= -nodefaultlibs -T "$(BASEDIR)\platform\devices\MPC5748G\linker\gcc\MPC5748G_ram.ld" --entry=Reset_Handler -Wl,-gc-sections
LDFLAGS_RAM+=-lgcc -lm -lc
LDFLAGS_FLASH:=-Wl,-Map=$(MAP_FLASH)
LDFLAGS_FLASH+= -nodefaultlibs -T "$(BASEDIR)\platform\devices\MPC5748G\linker\gcc\MPC5748G_flash.ld" --entry=Reset_Handler -Wl,-gc-sections
LDFLAGS_FLASH+=-lgcc -lm -lc
‍‍‍‍‍‍‍

And re-build the project.

Hope it helps.

Stan

0 Kudos
Reply

2,732 Views
lognight
Contributor III

Hi Stanislav,

 Yes. It worked, I can build it correctly by using gcc,very thans.

0 Kudos
Reply