Not able to generate code from Processor Expert file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to generate code from Processor Expert file

2,446 Views
amarjeet_kumar
Contributor II

Hi All

When I am Creating S32 DS Application project and selecting toolchan (Standard S32DS toolchain for ARM) with SDK (S32SDK_S32K14x_EAR_0.8.6) then I am able to generate processor expert code by keeping only SOSC_CLK.

 

Below is Configuration snapshot for the reference.

1.PNG

But When I am Creating S32 DS Application project and selecting toolchan (IAR Toolchain for ARM - (8.x)) with SDK (S32SDK_S32K1xx_RTM_3.0.0) then I am not able to generate processor expert code by keeping only SOSC_CLK.

 

Below is Configuration snapshot for the reference

Error Snapshot:

Please help me in solving this clock configuration problem.

Thanks

Amarjeet

0 Kudos
Reply
3 Replies

2,331 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Please re-upload last 2 snapshots. I see just some blanks.

Razvan

0 Kudos
Reply

2,332 Views
amarjeet_kumar
Contributor II

Hi Razvan

Please find here the 2 snapshots.

Configuration snapshot for the reference

1.jpg

Error Snapshot:

2.jpg

Thanks

Amarjeet

0 Kudos
Reply

2,331 Views
razva_tilimpea
NXP Employee
NXP Employee

Thanks,

Based on that error and would like to know how did you imported the project? It's a project started with EAR 0.8.6 and after that you switched the same project to RTM 3.0.0?

Could you provide me the steps to reproduce it on my side?

Best regards,

Razvan

0 Kudos
Reply