NXP MPC5748 Tcpip Stack component does not include

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MPC5748 Tcpip Stack component does not include

1,583 Views
pratikj_panchal
Contributor I

Hello,
I've a MPC5748 DevKit and I'm working in Ubuntu 18(x64).
IDE: S32 Design Studio.
In this IDE when I was add tcpip stack component then tcpip stack not include.

and got a following error :

tcpipstack_componet_error.png

and I'm working in Core : Z4_0.

Kindly tell what should I do for add tcpip stack component into my current project ?

Thanks & Regards,
Pratik Panchal

0 Kudos
Reply
1 Reply

1,496 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

based on release notes - SDK is fully supported on Windows host only. Under linux some components aren't working properly. 

Jiri

0 Kudos
Reply