MSCAN-Extended receive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MSCAN-Extended receive

1,257件の閲覧回数
pg31321
Contributor III

I can receive base CAN,and I can transmit extended  CAN.

but I can't receive extended CAN.

My program file is here:CAN2.0B.zip - Google Drive 

Config_CAN_MB (0, 0, RXDF, 0);  Can receive base CAN.

Config_CAN_MB (0, 0, RXDF, 2);  Can receive extended CAN. (see details in "MSCANID.h")

I give it the correct ID. but it seems to be filtered by the filter.

I have try to using REALTIMEBuffers to check ID which I give. It is correct .

Where did the error occur?

0 件の賞賛
返信
0 返答(返信)