MSCAN-Extended receive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MSCAN-Extended receive

1,249 次查看
pg31321
Contributor III

I can receive base CAN,and I can transmit extended  CAN.

but I can't receive extended CAN.

My program file is here:CAN2.0B.zip - Google Drive 

Config_CAN_MB (0, 0, RXDF, 0);  Can receive base CAN.

Config_CAN_MB (0, 0, RXDF, 2);  Can receive extended CAN. (see details in "MSCANID.h")

I give it the correct ID. but it seems to be filtered by the filter.

I have try to using REALTIMEBuffers to check ID which I give. It is correct .

Where did the error occur?

0 项奖励
回复
0 回复数