LPSPI and EDMA setting issue for the callback function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI and EDMA setting issue for the callback function

Jump to solution
6,298 Views
linton
Contributor II

linton_0-1714296358072.png

I am setting the SPI with S32DS configure tool, when I select the Transfer type DMA, and the Callback function is the SPI sent complete or the EDMA sent complete callback??  if this is the SPI transfer complete callback, Where to set the EDMA transfer complete callback? anybody know are there any doc for reference? I am confuse, Thanks

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
6,088 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Yes, that would be much more effective.

If the TX FIFO is written before the LPSPI module shifts the last word, there will be no gap between the frames.

 

BR, Daniel

View solution in original post

0 Kudos
Reply
9 Replies
6,278 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @linton,

You did not specify the MCU and the SDK version.

But this is a callback of the LPSPI driver.

 

The documentation of the driver can be accessed from the IDE

Right-click on the driver -> Documentation.

danielmartynek_0-1714392890631.png

 

Regards,

Daniel

0 Kudos
Reply
6,268 Views
linton
Contributor II

Thanks Daniel,

I check the relay doc you recommend, but still not clear.

the MCU I use is the S32K148_LQFP100, the SDK version is s32sdk_s32k1xx_rtm_401

 

0 Kudos
Reply
6,256 Views
danielmartynek
NXP TechSupport
NXP TechSupport

There is no other documentation for the drivers.

What issues fo you have with the callback?

The LPSPI driver should call the callback at the end of the transfer.

There is this SPI event defined in callbacks.h

danielmartynek_0-1714474808729.png

 

Regards,

Daniel

0 Kudos
Reply
6,183 Views
linton
Contributor II

Hi daniel,

I set the LPSPI_0 as below photo show:

linton_0-1715138116821.png

and I use the scope to test the SOUT waveform as below show:

linton_1-1715138558010.png

I send 20 bytes data, so I can calculate the baudrate is about 4.2M(what I set is 4.8M), and I check the clock is right. as below show:

linton_2-1715138789486.png

what cause this problem? what I need is 4.8M , 4.75 to 4.85 is acceptable. but 4.2M is bad.

 

the second problem is I change the transfer type from DMA to interrupt. the configure as below:

linton_3-1715139000238.png

and I also use the scope to test the SOUT waveform as below show:

linton_4-1715139066278.png

as you can see it separate my 20bytes data to five part, 4 bytes per part. What cause this problem?

linton_5-1715139340156.png

 

 

 

 

 

 

0 Kudos
Reply
6,154 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @linton,

The baudrate is calculated by the RTD driver from the LPSPI clock.

RM, 51.3.1.12 Clock Configuration Register (CCR).

Can you try using a higher freq. LPSPI clock?

It is expected to see some overhead when the interrupt mode is used, the LPSPI module has 4-word TX FIFO.

 

Regards,

Daniel

 

0 Kudos
Reply
6,135 Views
linton
Contributor II

Hi Daniel,

now I use the higher freq(56MHZ) as below show:

 

linton_0-1715518549516.png

linton_2-1715518674233.png

but the performance did not looks better than before, it still separate to five parts(4bytes per part):

the blue is using interrupt, the green is using DMA.

linton_4-1715519043643.png

are there any solution to solve this issue when I use the interrupt mode??

my application is simple as below show:

linton_5-1715519332199.png

linton_6-1715519431994.pnglinton_7-1715519460606.png

 

 

 

 

 

0 Kudos
Reply
6,097 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @linton,

This is simply a limitation of the driver.

In general, the SDK drivers are big and cause some CPU overhead.

Enabling the cache could somewhat help but not much.

 

Regards,

Daniel

 

0 Kudos
Reply
6,092 Views
linton
Contributor II

so to avoid this issue, I should not use the SDK interface, directly control the TDR?? 

0 Kudos
Reply
6,089 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Yes, that would be much more effective.

If the TX FIFO is written before the LPSPI module shifts the last word, there will be no gap between the frames.

 

BR, Daniel

0 Kudos
Reply