Issue of creating S32V234 APEX_graph

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue of creating S32V234 APEX_graph

939 次查看
751301185
Contributor II

微信图片_20200624151648.png

After I connected the kernel in Vision Graph and selected Processes in APEX2 Program Diagram, how should I choose Inlets (Image Inlet? or Number Inlet? or Pointer Inlet?), Outlets (Image Outlet? or Number Outlet ? or Pointer Outlet?)?

Can anyone help me analyze?

0 项奖励
回复
1 回复

881 次查看
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem modules is done only
via tickets. This Community is not appropriate for questions of this kind.  If you wish NXP

Technical Support to help you with this issue, please open a Support Case


Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复