Is there a way to use the S32K144x RTM SDK without Processor Expert?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a way to use the S32K144x RTM SDK without Processor Expert?

2,124件の閲覧回数
andrewstroz
Contributor I

I have tried to link the SDK .c files and include the .h files with no luck. What would be the best way to use the SDK without processor expert? or is there no way to do this?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,901件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello Andrew, 

well - theoretically it is possible use RTM SDK without processor expert, but you have to manually write all the config structures used in SDK as argument in functions.

For what reason you want bypass processor expert?  

Jiri

0 件の賞賛
返信

1,901件の閲覧回数
andrewstroz
Contributor I

No specific reason, was just looking into the possibility.

0 件の賞賛
返信