Is there API to get APEX2 consumption?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there API to get APEX2 consumption?

1,711件の閲覧回数
user123
Contributor I

When running an image processing on s32v234, I want to know consumption of APEX2 cores; for example, APEX2-0: XXX%, APEX2-1: XXX%.

Is there any API or the solution?

ラベル(2)
0 件の賞賛
返信
1 返信

1,659件の閲覧回数
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem modules is done only via tickets. This Community is not appropriate for questions of this kind. I will contact you by e-Mail with respect to this issue, for future requests, please

use only tickets.

 
Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信