How to use S32K144 FlexCan Interrupt to recieve can data?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use S32K144 FlexCan Interrupt to recieve can data?

跳至解决方案
4,602 次查看
victor_song_171
Contributor III

Just like the title.

I want to use FlexCan Interrupt to recieve can data with the S32DS.How could I do? What config and code have to do ?

PS : Just use S32DS IDE and s32k144 SDK,not simulink and IAR.

标签 (1)
1 解答
4,189 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are using the SDK, the CAN driver installs and calls interrupts upon each transmit/receive operation, you need not to do any further setup. Just you can install a user callback function which will be called from MB interrupt and you can distinguish between several events.

See more info about interrupts here;https://community.nxp.com/message/1045615 

BR, Petr 

在原帖中查看解决方案

4 回复数
4,190 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are using the SDK, the CAN driver installs and calls interrupts upon each transmit/receive operation, you need not to do any further setup. Just you can install a user callback function which will be called from MB interrupt and you can distinguish between several events.

See more info about interrupts here;https://community.nxp.com/message/1045615 

BR, Petr 

4,189 次查看
victor_song_171
Contributor III

thank you for the assistance. The issue is done.

0 项奖励
回复
4,189 次查看
victor_song_171
Contributor III

but how could i config the filter for recieved can id ?

0 项奖励
回复
4,189 次查看
PetrS
NXP TechSupport
NXP TechSupport
0 项奖励
回复