How to migrate the SDK from 0.8.4 to 0.8.6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to migrate the SDK from 0.8.4 to 0.8.6?

1,561 次查看
cheney
Contributor III

Dear support team:

      I've created a project using SDK 0.8.4, but now the latest version of SDK is 0.8.6. Is there any convenient way to migrate the SDK from 0.8.4 to 0.8.6?

IDE: S32DS v2.0 for ARM

MCU: S32k144

Thanks!

标记 (4)
0 项奖励
回复
1 回复

1,401 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately these two SDK versions aren't compatible. The only 100% working method is create new SDK project based on v0.8.6, move your code in this project and create new Processor Expert setting with values from previous version. 

I tried export PE settings and import it in the new version - but it works only partly. 

Jiri

0 项奖励
回复