How to Erase EEPROM partition in s32k146?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Erase EEPROM partition in s32k146?

跳至解决方案
1,512 次查看
s32k146_ige
Contributor IV

I was going through the example code for FlexRam as EEPROM and NVM partition. the code does demonstrate how to write in EEPROM partition, but there is no erase operation or erase code to erase EEPROM partition.

i tried using following function,

 

address = flashSSDConfig.EERAMBase;

ret = FLASH_DRV_EraseSector(&flashSSDConfig, address, 8);
DEV_ASSERT(STATUS_SUCCESS == ret);

 

Also I was not able to write in NVM Partition, why the code checks for EEPROM size for NVM write ?

 

This is the example code,

 

/*
 * Copyright (c) 2015 - 2016 , Freescale Semiconductor, Inc.
 * Copyright 2016-2018 NXP
 * All rights reserved.
 *
 * THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
 * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
 * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
 * IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
 * INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
 * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
 * STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
 * IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
 * THE POSSIBILITY OF SUCH DAMAGE.
 */

/* MODULE main */

/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "clockMan1.h"
#include "Flash.h"


volatile int exit_code = 0;
/* User includes (#include below this line is not maintained by Processor Expert) */

#include <stdint.h>
#include <stdbool.h>

/* Declare a FLASH config struct which initialized by FlashInit, and will be used by all flash operations */
flash_ssd_config_t flashSSDConfig;

/* Data source for program operation */
#define BUFFER_SIZE         0x100u          /* Size of data source */
uint8_t sourceBuffer[BUFFER_SIZE];

/* Function declarations */
void CCIF_Handler(void);
/* If target is flash, insert this macro to locate callback function into RAM */
START_FUNCTION_DECLARATION_RAMSECTION
void CCIF_Callback(void)
END_FUNCTION_DECLARATION_RAMSECTION

/*!
  \brief The main function for the project.
  \details The startup initialization sequence is the following:
 * - startup asm routine
 * - main()
*/
int main(void)
{
  /* Write your local variable definition here */
    status_t ret;        /* Store the driver APIs return code */
    uint32_t address;
    uint32_t size;
    uint32_t failAddr;
    uint32_t i;
    flash_callback_t pCallBack;
#if (FEATURE_FLS_HAS_PROGRAM_PHRASE_CMD == 1u)
#ifndef FLASH_TARGET
    uint8_t unsecure_key[FTFx_PHRASE_SIZE] = {0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFEu, 0xFFu, 0xFFu, 0xFFu};
#endif
#else   /* FEATURE_FLASH_HAS_PROGRAM_LONGWORD_CMD */
    uint8_t unsecure_key[FTFx_LONGWORD_SIZE] = {0xFEu, 0xFFu, 0xFFu, 0xFFu};
#endif  /* FEATURE_FLS_HAS_PROGRAM_PHRASE_CMD */

  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  #ifdef PEX_RTOS_INIT
    PEX_RTOS_INIT();                   /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of Processor Expert internal initialization.                    ***/

  /* Write your code here */

    /* Initialize and configure clocks
     *  -   see clock manager component for details
     */
    CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
            g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
    CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);

    /* Init source data */
    for (i = 0u; i < BUFFER_SIZE; i++)
    {
        sourceBuffer[i] = i;
    }

    /* Disable cache to ensure that all flash operations will take effect instantly,
     * this is device dependent */
#ifdef S32K146_SERIES
    MSCM->OCMDR[0u] |= MSCM_OCMDR_OCM1(0xFu);
    MSCM->OCMDR[1u] |= MSCM_OCMDR_OCM1(0xFu);
    MSCM->OCMDR[2u] |= MSCM_OCMDR_OCM1(0xFu);
#endif /* S32K146_SERIES */

    /* Install interrupt for Flash Command Complete event */
    INT_SYS_InstallHandler(FTFC_IRQn, CCIF_Handler, (isr_t*) 0);
    INT_SYS_EnableIRQ(FTFC_IRQn);

    /* Enable global interrupt */
    INT_SYS_EnableIRQGlobal();

    /* Always initialize the driver before calling other functions */
    ret = FLASH_DRV_Init(&Flash_InitConfig0, &flashSSDConfig);
    DEV_ASSERT(STATUS_SUCCESS == ret);

#if ((FEATURE_FLS_HAS_FLEX_NVM == 1u) & (FEATURE_FLS_HAS_FLEX_RAM == 1u))
    /* Config FlexRAM as EEPROM if it is currently used as traditional RAM */
    if (flashSSDConfig.EEESize == 0u)
    {
#ifndef FLASH_TARGET
        /* First, erase all Flash blocks if code is placed in RAM to ensure
         * the IFR region is blank before partitioning FLexNVM and FlexRAM */
        ret = FLASH_DRV_EraseAllBlock(&flashSSDConfig);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Verify the erase operation at margin level value of 1 */
        ret = FLASH_DRV_VerifyAllBlock(&flashSSDConfig, 1u);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Reprogram secure byte in Flash configuration field */
#if (FEATURE_FLS_HAS_PROGRAM_PHRASE_CMD == 1u)
        address = 0x408u;
        size = FTFx_PHRASE_SIZE;
#else   /* FEATURE_FLASH_HAS_PROGRAM_LONGWORD_CMD == 1u */
        address = 0x40Cu;
        size = FTFx_LONGWORD_SIZE;
#endif /* FEATURE_FLS_HAS_PROGRAM_PHRASE_CMD */
        ret = FLASH_DRV_Program(&flashSSDConfig, address, size, unsecure_key);
        DEV_ASSERT(STATUS_SUCCESS == ret);
#endif /* FLASH_TARGET */

        /* Configure FlexRAM as EEPROM and FlexNVM as EEPROM backup region,
         * DEFlashPartition will be failed if the IFR region isn't blank.
         * Refer to the device document for valid EEPROM Data Size Code
         * and FlexNVM Partition Code. For example on S32K146:
         * - EEEDataSizeCode = 0x02u: EEPROM size = 4 Kbytes
         * - DEPartitionCode = 0x08u: EEPROM backup size = 64 Kbytes */
        ret = FLASH_DRV_DEFlashPartition(&flashSSDConfig, 0x02u, 0x08u, 0x0u, false, true);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Re-initialize the driver to update the new EEPROM configuration */
        ret = FLASH_DRV_Init(&Flash_InitConfig0, &flashSSDConfig);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Make FlexRAM available for EEPROM */
        ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_ENABLE, 0x00u, NULL);
        DEV_ASSERT(STATUS_SUCCESS == ret);
    }
    else    /* FLexRAM is already configured as EEPROM */
    {
        /* Make FlexRAM available for EEPROM, make sure that FlexNVM and FlexRAM
         * are already partitioned successfully before */
        ret = FLASH_DRV_SetFlexRamFunction(&flashSSDConfig, EEE_ENABLE, 0x00u, NULL);
        DEV_ASSERT(STATUS_SUCCESS == ret);
    }
#endif /* (FEATURE_FLS_HAS_FLEX_NVM == 1u) & (FEATURE_FLS_HAS_FLEX_RAM == 1u) */

    /* Set callback function before a long time consuming flash operation
     * (ex: erasing) to let the application code do other tasks while flash
     * in operation. In this case we use it to enable interrupt for
     * Flash Command Complete event */
    pCallBack = (flash_callback_t)CCIF_Callback;
    flashSSDConfig.CallBack = pCallBack;

    /* Erase the sixth PFlash sector */
    address = 6u * FEATURE_FLS_PF_BLOCK_SECTOR_SIZE;
    size = FEATURE_FLS_PF_BLOCK_SECTOR_SIZE;
    ret = FLASH_DRV_EraseSector(&flashSSDConfig, address, size);
    DEV_ASSERT(STATUS_SUCCESS == ret);

    /* Disable Callback */
    flashSSDConfig.CallBack = NULL_CALLBACK;

    /* Verify the erase operation at margin level value of 1, user read */
    ret = FLASH_DRV_VerifySection(&flashSSDConfig, address, size / FTFx_DPHRASE_SIZE, 1u);
    DEV_ASSERT(STATUS_SUCCESS == ret);

    /* Write some data to the erased PFlash sector */
    size = BUFFER_SIZE;
    ret = FLASH_DRV_Program(&flashSSDConfig, address, size, sourceBuffer);
    DEV_ASSERT(STATUS_SUCCESS == ret);

    /* Verify the program operation at margin level value of 1, user margin */
    ret = FLASH_DRV_ProgramCheck(&flashSSDConfig, address, size, sourceBuffer, &failAddr, 1u);
    DEV_ASSERT(STATUS_SUCCESS == ret);

    /* Try to write data to EEPROM if FlexRAM is configured as EEPROM */
    if (flashSSDConfig.EEESize != 0u)
    {
        address = flashSSDConfig.EERAMBase;
        size = sizeof(uint32_t);
        ret = FLASH_DRV_EEEWrite(&flashSSDConfig, address, size, sourceBuffer);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Verify the written data */
        if (*((uint32_t *)sourceBuffer) != *((uint32_t *)address))
        {
            /* Failed to write data to EEPROM */
            exit_code = 1u;
            return exit_code;
        }

        /* Try to update one byte in an EEPROM address which isn't aligned */
        address = flashSSDConfig.EERAMBase + 1u;
        size = sizeof(uint8_t);
        sourceBuffer[0u] = 0xFFu;
        ret = FLASH_DRV_EEEWrite(&flashSSDConfig, address, size, sourceBuffer);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Then verify */
        if (sourceBuffer[0u] != *((uint8_t *)address))
        {
            /* Failed to update data to EEPROM */
            exit_code = 1u;
            return exit_code;
        }
    }
    else
    {
#if (FEATURE_FLS_HAS_FLEX_NVM == 1u)
        /* Erase a sector in DFlash */
        address = flashSSDConfig.DFlashBase;
        size = FEATURE_FLS_DF_BLOCK_SECTOR_SIZE;
        ret = FLASH_DRV_EraseSector(&flashSSDConfig, address, size);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Verify the erase operation at margin level value of 1, user read */
        ret = FLASH_DRV_VerifySection(&flashSSDConfig, address, size / FTFx_PHRASE_SIZE, 1u);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Write some data to the erased DFlash sector */
        address = flashSSDConfig.DFlashBase;
        size = BUFFER_SIZE;
        ret = FLASH_DRV_Program(&flashSSDConfig, address, size, sourceBuffer);
        DEV_ASSERT(STATUS_SUCCESS == ret);

        /* Verify the program operation at margin level value of 1, user margin */
        ret = FLASH_DRV_ProgramCheck(&flashSSDConfig, address, size, sourceBuffer, &failAddr, 1u);
        DEV_ASSERT(STATUS_SUCCESS == ret);
#endif /* FEATURE_FLS_HAS_FLEX_NVM */
    }

  /*** Don't write any code pass this line, or it will be deleted during code generation. ***/
  /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
  #ifdef PEX_RTOS_START
    PEX_RTOS_START();                  /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of RTOS startup code.  ***/
  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
  for(;;) {
    if(exit_code != 0) {
      break;
    }
  }
  return exit_code;
  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/

/* END main */
/*!
** @}
*/

/*!
  \brief Interrupt handler for Flash Command Complete event
*/
void CCIF_Handler(void)
{
    /* Disable Flash Command Complete interrupt */
    FTFx_FCNFG &= (~FTFx_FCNFG_CCIE_MASK);

    return;
}

/*!
  \brief Callback function for Flash operations
*/
START_FUNCTION_DEFINITION_RAMSECTION
void CCIF_Callback(void)
{
    /* Enable interrupt for Flash Command Complete */
    if ((FTFx_FCNFG & FTFx_FCNFG_CCIE_MASK) == 0u)
    {
        FTFx_FCNFG |= FTFx_FCNFG_CCIE_MASK;
    }
}
END_FUNCTION_DEFINITION_RAMSECTION

/*
** ###################################################################
**
**     This file was created by Processor Expert 10.1 [05.21]
**     for the Freescale S32K series of microcontrollers.
**
** ###################################################################
*/

 

 

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,487 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

A partition can be erased only by mass erase operation. Then it acts as blank new device and user can write new partition.

在原帖中查看解决方案

1 回复
1,488 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

A partition can be erased only by mass erase operation. Then it acts as blank new device and user can write new partition.