HOWTO: Create the Blinking LED example project using S32K144 SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HOWTO: Create the Blinking LED example project using S32K144 SDK

2,963 次查看
Swaroop_joshi
Contributor I

hello, 

we had interesting to find the Article of the "HOWTO: Create the Blinking LED example project using S32K144 SDK", we had got the step for our Board S32K148 SDK for the debugging of the project.  

Swaroop_joshi_0-1674458449229.png

But We didn't get the any S32K148 SDK of the RTM2.0.0 

Swaroop_joshi_1-1674458616098.png

 So please Suggest how to resolve the issue or Please Send the Relevant S32K148 SDK of the RTM2.0.0 

 

waiting for that 

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,952 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

why RTM2.0.0 is needed? Latest one in S32DS2.2 is RTM3.0.3 
So what is your option available when selecting SDK in project?
Be sure all needed packages are installed 

PetrS_0-1674466841058.png
And when creating project a GNU toolchain v.6.3 is selected in the first step, which is required by SDK, so it can be selected in the next step.

BR, Petr

 

0 项奖励
回复

2,950 次查看
Swaroop_joshi
Contributor I
Hello,
I had use the workspace of S32 DESIGN STUDIO.ARM.2018.R1 and create the S32DS Design DS project of blinking with select the processors- S32K148.
here installation steps, we already taken the GNU toolchain v.6.3 in the first step but we didn't see the any relevant SDK For processors- S32K148.

so we confuges, can we use the debugger for this NXP S32 K148 EV Board? or any other SDK required for that.
0 项奖励
回复

2,945 次查看
Swaroop_joshi
Contributor I

hello, 

 

we followed all Blinking step as per LED example project using S32K148 SDK,

but again, we stuck at the point of the error.

Screenshot (46).png

 

 

0 项奖励
回复

2,930 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try demo examples, either SDK based or baremetal one, if the launch error still exist for prepared project as well.

BR, Petr

0 项奖励
回复