Flash DRV erasesector in SDK s32k1xx 15 does not execute correctly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash DRV erasesector in SDK s32k1xx 15 does not execute correctly

1,198 Views
561999181
Contributor I

Flash DRV erasesector in SDK s32k1xx 15 does not execute correctly

When the program executes to the following code, the function cannot be executed

/* Calling flash command sequence function to execute the command */
ret = FLASH_DRV_CommandSequence(pSSDConfig);

0 Kudos
Reply
1 Reply

1,095 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Yang,

At first, I would like to ask you a few questions.

Which concrete MCU do you use?

Which SDK version and S32 Design Studio do you use?

What are the parameters such as the address and size of the erase sector function (FLASH_DRV_EraseSector)?

Can you share your code?

Thank you.

Best Regards,

Diana

0 Kudos
Reply