Error for SDK-Pin_mux Functional Properties

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error for SDK-Pin_mux Functional Properties

3,367 Views
leekate-b45752
NXP Employee
NXP Employee

Hello, 

The customer is using S32 DS v1.3 and an example of SDK RTM v1.3, but when they clicked the pin_mux, they couldn't configuration in 'Functional Properties' as below. 

Could you check this symptom?

pastedImage_1.png

Best regards,

Kate Lee

0 Kudos
Reply
4 Replies

2,836 Views
cezardobromir
NXP Employee
NXP Employee

Hello Kate,

This issue is currently under investigation as it has also been reported here:

https://community.nxp.com/thread/453118 

We will come with an update on the issue as soon as we identify the root cause

Best Regards,

Cezar

0 Kudos
Reply

2,836 Views
sohyunjang
Contributor III

Hi, I have same problem in Functional Properties at S32DS ver1.3.

Has this problem been resolved?

Thank you.

0 Kudos
Reply

2,836 Views
cezardobromir
NXP Employee
NXP Employee

Hello Sohyun,

Yes, this problem has been fixed in S32 SDK EAR 0.8.5. All the versions form this one to the present display the correct information in the Functional Properties tab

Best regards,

Cezar

0 Kudos
Reply

2,836 Views
jeremiahg
Contributor III

Cezar,

Thanks for the update. Hopefully NXP can address this quickly. I have to add code manually in main.c to temporary fixes to two projects because I cannot alter the Functional Properties.

Regards,

Jeremiah

0 Kudos
Reply