Error : Error in ONCE status register during instruction execution.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error : Error in ONCE status register during instruction execution.

4,339 次查看
fu860925
Contributor I

MPC5744P:NXP\S32DS_Power_v2017.R1\S32DS\S32_SDK_MPC574xx_BETA_0.9.0\examples\MPC5744P\driver_examples\system\fccu_fault_injection

pastedImage_1.png

pastedImage_2.png

标签 (1)
0 项奖励
回复
2 回复数

3,755 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

from the figures you posted above I cannot determine, if you have installed all S32DS updates, but this error appeared when the newest pemicro debug interface had not been installed.

Please install the newest update 9 and let me know, if this resolved your problem.

https://community.nxp.com/docs/DOC-342355?sr=search&searchId=93f9b31d-9198-405b-8487-1e2c7e543572&se... 

Regards,

Martin

0 项奖励
回复

3,499 次查看
bingwang312
Contributor III

I am surprised to see exactly same issue happened 3 years ago. I installed S32DS PA V2.1 + SDK RTM 3.0.3, updated all component according to its checklist to the newest versions. but when I tried several examples from SDK 3.0.3,  all examples failed on debugging,  same errors of "ONCE status register..........". does anyone have a clue on this ? how to fix the problem? I guess it is about the complier or ASM code some where wrong. it seems a pointer of instructions always goes wrong place.

bingwang312_0-1639167391908.png

bingwang312_0-1639167549293.png

 

 

0 项奖励
回复