Enable LWIP without FreeRTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable LWIP without FreeRTOS

2,315 次查看
rajani_sureja33
Contributor III

Hi,

I am using s32 design studio for NXP MPC5748G dev kit. Here LWIP example code "lwip_mpc5748g" integrated with freertos by default.

So what should i do to run this example without  freertos?

Regards,

Rajani Sureja

Embedded FW Enginner 

0 项奖励
回复
4 回复数

2,130 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I received following question from example author:

It is possible to run the example without RTOS and it is also pretty simple. Please do following steps:

+ Import example lwip_mpc5748g as normal

+ In Processor Expert tool, just delete/remove FreeRTOS component

+ Generate code again

Now, it should work again without FreeRTOS.

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 项奖励
回复

1,700 次查看
晶晶
Contributor I

Hi Martin,

Would you pls. give me a demo project with lwip without freertos?

In my trial, I cannot ping with the lwip demo without freertos. 

Thanks a lot.

0 项奖励
回复

2,130 次查看
rajani_sureja33
Contributor III

Thanks Martin!!

0 项奖励
回复

2,130 次查看
rajani_sureja33
Contributor III

would you please reply to my queries for question

How to use printf function in S32DS for Power Architecture for MPC5748G

0 项奖励
回复