Hi @ozgrdmo
The "Functional Groups" feature in S32 Design Studio provides an efficient way to configure functions and manage code generation. With this feature, you can customize several options for each function. You can specify the generated function name, select the core (for multicore processors only) that is affecting the generated source code, or write a function description (this description is generated in the C file). You can also add, copy, and remove functional groups as needed.
For more detailed information, refer to the S32DS Help section under Help Contents.
BR, VaneB