Cannot find required include files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot find required include files

1,897件の閲覧回数
roger_davis
Contributor II

I downloaded S32SDK_S32_PA_RTM_3.0.3.exe.  I then imported one of the examples into my workspace, C:\NXP\S32_SDK_S32_PA_RTM_3.0.3\examples\MPC5744P\driver_examples\timer\pit_periodic_interrupt.

When I tried to build it, main.c is looking for several include files that don't exist anywhere in the SDK.  For example, Cpu.h, pin_mux.h, pit1.h, clockMan1.h.

Where should I look for these files?

ラベル(1)
0 件の賞賛
返信
1 返信

1,891件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi roger_davis,

Please click Generate Processor Expert Code:

Generate Processor Expert Code.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信