CSEc key load result

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSEc key load result

3,125件の閲覧回数
yqs77
Contributor II

As I known, the CSEc key will be loaded in the format of M1, M2, M3, and the M4, M5 are used to check the result of key load. It is safe for that the calculation is irreversible, but I want to know that after loading the key to CSEc slot, whether the key is decrypted or still stored as the format of M1 to M5?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,114件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it follows SHE specification:

lukaszadrapa_0-1655962241999.png

 Regards,

Lukas

0 件の賞賛
返信

3,069件の閲覧回数
yqs77
Contributor II

Thanks for the reply. Refer to the attachment, I will suppose that when the key like BOOT_MAC_KEY loaded to slot, it will be encrypted with the AES in ECB mode. And when it used like BOOT_MAC calculation, it is still read in AES encrypted form. Am I correct?

0 件の賞賛
返信

3,026件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm sorry for delayed response.

From user's point of view, this is completely hidden to user. A user can use the keys or BOOT_MAC as needed and knowledge of these background operations is not needed. It follows SHE specification to ensure the keys / BOOT_MAC are protected as required. We can't share more details.

Regards,

Lukas

0 件の賞賛
返信