Application processor (A53) CPU Utilization when using endocder (H.264) in a graph running in S32V23

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application processor (A53) CPU Utilization when using endocder (H.264) in a graph running in S32V23

Jump to solution
3,710 Views
mrosar11
Contributor IV

Hi, we need help to understand why the CPU utilization in the application processor (A53) is higher than expected when using the encoder as part of the graph. Based on our observations and analysis using the QNX Momentics IDE, there are thread events yielding a higher utilization than expected on the A53. From what we can tell, opening the encoder driver (H.264 driver) spawns these threads. We need help to see how we can reduce this CPU utilization.

I would like to setup a call with someone familiar with these details.

Labels (1)
0 Kudos
Reply
1 Solution
4 Replies
3,580 Views
mrosar11
Contributor IV
0 Kudos
Reply
3,549 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @mrosar11,

Thanks for letting me know you were able to move your post to the right community. I will mark your answer as an accepted solution.

 

Best regards 

0 Kudos
Reply
3,633 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @mrosar11,

 To receive the best support please post this question in the internal community best suited for your project, I am aware that your company has several internal communities.

If you are unsure the community on which this question should be posted please contact your FAE/NXP representative, they should be able to guide you in that matter.

In case you don't have the FAE/NXP representative contact please let me know so I can help you with that.

 

Thanks in advance.

0 Kudos
Reply
3,695 Views
mrosar11
Contributor IV
 
 

Untitled.gifUntitled.gif

0 Kudos
Reply