Application processor (A53) CPU Utilization when using endocder (H.264) in a graph running in S32V23

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Application processor (A53) CPU Utilization when using endocder (H.264) in a graph running in S32V23

跳至解决方案
3,806 次查看
mrosar11
Contributor IV

Hi, we need help to understand why the CPU utilization in the application processor (A53) is higher than expected when using the encoder as part of the graph. Based on our observations and analysis using the QNX Momentics IDE, there are thread events yielding a higher utilization than expected on the A53. From what we can tell, opening the encoder driver (H.264 driver) spawns these threads. We need help to see how we can reduce this CPU utilization.

I would like to setup a call with someone familiar with these details.

标签 (1)
0 项奖励
回复
1 解答
3,675 次查看
mrosar11
Contributor IV
0 项奖励
回复
4 回复数
3,676 次查看
mrosar11
Contributor IV
0 项奖励
回复
3,645 次查看
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @mrosar11,

Thanks for letting me know you were able to move your post to the right community. I will mark your answer as an accepted solution.

 

Best regards 

0 项奖励
回复
3,729 次查看
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @mrosar11,

 To receive the best support please post this question in the internal community best suited for your project, I am aware that your company has several internal communities.

If you are unsure the community on which this question should be posted please contact your FAE/NXP representative, they should be able to guide you in that matter.

In case you don't have the FAE/NXP representative contact please let me know so I can help you with that.

 

Thanks in advance.

0 项奖励
回复
3,791 次查看
mrosar11
Contributor IV
 
 

Untitled.gif

 

0 项奖励
回复