Adding Data to Specific Memory Area

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding Data to Specific Memory Area

Jump to solution
3,939 Views
dsilva
Contributor III

Hello.

I need to add some values in a specific area of s32k144 memory. I'm using s32ds 2.2.

I added a new area definition to the linker as follows:

"m_appheader(RX) : ORIGIN = 0x00006800, LENGTH = 0x00000400"

In the main.c file I added the following line:

__atribute__ ((section(".appheader"))) const FLASH_APPHEADER_INFO APP_HEADER ={ ...DATA...};

The compilation runs without errors, the appheader appears in the map file, but when opening the hex or bin the data was not added. The entire appheader region is set to 0xFF.

Is there any configuration needed in the compilation so that this data is not removed?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,925 Views
dsilva
Contributor III

I founded the problem.

I was just adding the appheader in the MEMORY field, the addition in the SECTION field was missing.

View solution in original post

0 Kudos
Reply
3 Replies
3,926 Views
dsilva
Contributor III

I founded the problem.

I was just adding the appheader in the MEMORY field, the addition in the SECTION field was missing.

0 Kudos
Reply
3,931 Views
Joey_van_Hummel
Contributor IV

I assume it has to do with your APP_HEADER being constant and thus the access to the .appheader region is being optimized away.

0 Kudos
Reply
3,929 Views
dsilva
Contributor III

Hello,

 

I removed the "const" and it didn't work.

 

I also added an ''IF" to that const and it didn't work too.

0 Kudos
Reply