using S32K144 EVB as JTAG to debug other S32K144 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using S32K144 EVB as JTAG to debug other S32K144 chip

1,554 Views
lyp06118022
Contributor I

Hi,

I have a NXP s32k144 EVB, it works normal. Now i designed my own S32K144 board, and i have tried Multilink to debug it. it is OK. However, the Multilink is shared. So i want to use EVB's JTAG interface( J12, SDA jtag interface). 

First, i  pick out the U7, U10 to make openSDA disconnect with the EVB S32k144 chip, then i tried the J12 interface with my new s32k144 board, the "P&E connection assistant" window occurs, it says "an error occurs while connecting to the interface hardware" the openSDA can be recognized.

Then i picked out the S32K144 chip from the EVB board. But the S32DS IDE still can not debug. the error is the same. 

So i want to know what should i do to make it work as a JTAG. i have read the link

"Using the Freedom Board as SWD Programmer".  Thank you.

Regards,

Yanpo, li

Labels (1)
0 Kudos
Reply
1 Reply

1,488 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, it is definitely possible. Is your board powered? Please check board schematic if it is connected properly to your EVB - https://www.nxp.com/downloads/en/schematics/S32K144EVB-SCH-29248-RB.pdf   

Hope it helps. 

Jiri

0 Kudos
Reply