the variable was defined in the GRAM region

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the variable was defined in the GRAM region

1,422 Views
wangjianpeng
Contributor I

I used S32DS to debug MAC57D54H and found that the variable was defined in the GRAM region. I checked the link file and found that it was written like this:

MEMORY {
FLASH_CONFIG : ORIGIN = 0x18f9c000, LENGTH = 16K
FLASH_CODE : ORIGIN = 0x19000000, LENGTH = 0x280000
CODE_A5 : ORIGIN = 0x19280000, LENGTH = 0x80000
GRAM : ORIGIN = 0x3F000000 + 0x100, LENGTH = 1M - 0x100 - 256K
IOP_RAM : ORIGIN = 0x3E400000, LENGTH = 32K
}

__DATA_ROM = .; /* Symbol is used by startup for data initialization */


.data : AT(__DATA_ROM)
{
. = ALIGN(4);
__DATA_RAM = .;
__data_start__ = .; /* create a global symbol at data start */
*(.data*)
__DATA_END = .;
__data_end__ = .; /* define a global symbol at data end */
} > GRAM

__DATA_END = __DATA_ROM + (__data_end__ - __data_start__);

.bss ALIGN(16) :
{
_BSS_BEGIN = .;
__bss_start__ = .;
*(.bss*) /* Zero-filled run time allocate data memory */
*(COMMON)
__bss_end__ = .;
_BSS_END = .;
} > GRAM


/* stack and heap shall be located in the same memory region */
.heap ALIGN(8):
{
__end__ = .;
PROVIDE(_end = .);
PROVIDE(end = .);
. += HEAP_SIZE;
} > GRAM

.stack ALIGN(8):
{
_stack_s = .;
. += STACK_SIZE;
_stack_e = .;
} > GRAM

In my understanding, the GRAM area is the area of 2D-ACE to display the image information, So I want to know what I should do?

Thank you!

Tags (2)
0 Kudos
Reply
1 Reply

1,354 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks like that this linker file is standard one for M4 core and there is no mapped SRAM for that core. All SRAM is used by A5 and M0 core. Am I right? You can check linker files for other cores in your project. 

You can normally use it as it is - if you  are not facing any issues. Otherwise - you need to shring SRAM from M0 or A5 core and use available memory for M4 and put there stack/heap and other stuff.  

Jiri

0 Kudos
Reply