the ethernet example about the MPC5748g

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

the ethernet example about the MPC5748g

跳至解决方案
2,329 次查看
961271210
Contributor I

This project is based on the example project enet_rmii_udp. I use mpc5748G to debug it. There aren't any problems in the code, but the S32 always tells me there is problem about the enet_rmii_udp.elf. So I wonder if I use some wrong setting in the debug. 

pastedImage_1.png

This is what I use in the debug setting.

pastedImage_2.png

pastedImage_3.png

What is the problem ?

Thanks,

Jupeng

0 项奖励
回复
1 解答
2,199 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I imported your project and there is problem with Path to additional elf files. In my case - all 3 core projects are located directly in Workspace root folder. Removing enet_rmii_udp from path should solve your issue. 

pastedImage_1.png

Jiri

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,200 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I imported your project and there is problem with Path to additional elf files. In my case - all 3 core projects are located directly in Workspace root folder. Removing enet_rmii_udp from path should solve your issue. 

pastedImage_1.png

Jiri

0 项奖励
回复