the error"first defined here

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the error"first defined here

2,112件の閲覧回数
609510318
Contributor I

S32 Design Studio for Arm.when the project was built all firstly, the error"first defined here" was happened,what is the reason? 

Notes:The lib file contained the functions with the error. Was the way that the lib was input into the project is wrong?

Thanks for your answer

タグ(2)
0 件の賞賛
返信
1 返信

2,021件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your project? It is an included example? Can you shared output from build console? 

Jiri 

0 件の賞賛
返信