the error"first defined here

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the error"first defined here

2,116 Views
609510318
Contributor I

S32 Design Studio for Arm.when the project was built all firstly, the error"first defined here" was happened,what is the reason? 

Notes:The lib file contained the functions with the error. Was the way that the lib was input into the project is wrong?

Thanks for your answer

0 Kudos
Reply
1 Reply

2,025 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your project? It is an included example? Can you shared output from build console? 

Jiri 

0 Kudos
Reply