sprintf bug when using newlib nano with "-u _printf_float" linker option

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sprintf bug when using newlib nano with "-u _printf_float" linker option

8,424 次查看
dan_teodorescu
Contributor III

Hello,

I am using S32 Design Studio 2017.R1 for an MPC5777C project. Because of the embedded real-time nature of our project, we are using S32DS newlib nano as the standard "C" library. By default this library does not provide support for sprintf floating point format specifiers, unless "-u _printf_float" is added as a linker command line option.

I added the linker command line option mentioned above, but sprintf() does not work as expected. In my test code the contents of buffer are "nan xyz", instead of "1.0 xyz" right after the call to sprintf() returns.

int main()
{
    char buffer [256];
    sprintf(buffer, "%f xyz", 1.0f);
    counterclass myccounter;

    xcptn_xmpl (); /* Configure and Enable Interrupts */

    /* Loop forever */
    for(;;) {
        myccounter.increment();
    }
}

I have attached my test project, including the code above, newlib.c (which resolves the missing syscalls that newlib expects), and the compiler/linker settings.

I saw similar behavior in our actual application. In that project I narrowed down the issue to variable _fpvalue getting a value of 0xFFFFFFFFFFFFFFFF in _printf_float (nano-vfprintf_float.c).

int
_printf_float (struct _reent *data,
        struct _prt_data_t *pdata,
        FILE * fp,
        int (*pfunc) (struct _reent *, FILE *, _CONST char *,
        size_t len), va_list * ap)
{

    /* ... */

    if (pdata->flags & LONGDBL)
    {
        _fpvalue = (double) GET_ARG (N, *ap, _LONG_DOUBLE);
    }
    else
    {
        _fpvalue = GET_ARG (N, *ap, double);

        /* _fpvalue is now 0xFFFFFFFFFFFFFFFF even though argument to sprintf was 1.0f. */
    }

    /* ... */

}

Has anyone seen this issue and is there a fix for it?

Thank you

0 项奖励
回复
2 回复数

7,823 次查看
dan_teodorescu
Contributor III

Hi Alexander,

I upgraded to "S32 Design Studio for Power Architecture 2017.R1 Updates 5 SDK MPC574xx RTM 1.0.0 and Update 6 Service Pack MPC5775x" and I no longer see the issue. Since my configuration excludes dynamic memory allocation, newlib sprintf() cannot generate the textual representation. This is a known limitation of how newlib implements converting floating point values to string. However, the new behavior matches my expectation so this issue can be closed.

Thank you for your support.

Dan

0 项奖励
回复

7,823 次查看
alexanderfedoto
NXP Employee
NXP Employee

Hello

Have you tried to install Update 2 ? S32 Design Studio for Power Architecture 2017.R1 - Update 2 available 

This update also contains newer GCC version including fix newlib nano.

#CMPE200GCC-126

CMPE200GCC-178

0 项奖励
回复